The standard way to generate a header file with MLC register settings is to generate from decision-tree .txt file (exportet from WEKA or python).In our project we want to avoid tool interaction.The register settings (ucf or header file) should be gen...
Is it possible to use accelerometer in low power-, or ultra-low power mode in combinationwith MLC?All current calculations, i found were based on the 170µA of accelerometer in high performance mode.
Hi Eleon BORLINI, thanks for the answer!Ok, i understand that i have to pay attention on the right ODR of the accelerometer.You also wrote that data patterns come from accelerometer and gyro sensors, and that the MLC consumtion is only a small fracti...