Edge AI

Ask questions and find answers on how to deploy, debug, and optimize AI models on ST microcontrollers, microprocessors, and smart sensors.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Unico feature calculation

Hello,I'm trying to figure out how Unico calculates it feature values during .arff creation.Unfortunately, if I calculate the features as described in AN5804, the feature values differ from the Unico output.I have attached two files, accelerometer sa...

He_Ka by Associate
  • 1944 Views
  • 2 replies
  • 0 kudos

stm32cube_ai, airun(),The output data is abnormal

When I use a function 【int ai_run(const void *in_data, void *out_data)】to make predictions,the out_data always output【0】No matter how I change the value of the input data, the value of the output data will not change, it will always be 0.int ai_run(c...

屏幕截图(315).png
Sunjing by Associate II
  • 1285 Views
  • 1 replies
  • 0 kudos

Error while configuring activations with X-CUBE-AI

I am trying to create an AI App with X-CUBE-AI but I encountered the following error:TEMPLATE - Error create_and_init type=0x30 code=0x13I have not touched the code yet so it is really frustrating. If I comment the line "MX_X_CUBE_AI_Init();" the cod...

Resolved! Modifying an existing program in FP-AI-VISION1 for STM32H747i-DISCO

Hi,I'm doing a university project on top down people counting and the existing People Counting program in the FP-AI-VISION1 package seems perfect. I'm new to microcontrollers and AI, generally speaking, but I just wanted to know if it was possible to...

DarrinR1 by Associate II
  • 986 Views
  • 2 replies
  • 0 kudos

STM32Cube.AI runtime won't work

I'm trying to add different trained models to my CubeMX project, but all Keras and ONNX models (even example models from the stm model zoo) produce the same error during the analization process:  Failed to execute script 'pyi_rth_pkgres' due to unhan...

M_Ehe by Associate II
  • 2092 Views
  • 4 replies
  • 0 kudos

STM32CubeAI Application template: Change input type

Hello,I'm new to C and STM32 deployment. I am developing a ML model that I would like to run on a STM32F446RE board. I'm using STM32CubeIDE 1.14.0 and X-Cube-AI 8.1.0. I followed the first steps to add the model, Analyze and Validate on desktop and o...

Elo by Associate
  • 1210 Views
  • 2 replies
  • 1 kudos

Resolved! FP-AI-VISION1 compile issue

Hi ST professional team Following the documentation  instructions & opteratingHow to use Teachable Machine to create an image classification application on STM32 https://wiki.stmicroelectronics.cn/stm32mcu/wiki/AI:How_to_use_Teachable_Machine_to_crea...

111.jpg
cvd_pony by Associate
  • 2005 Views
  • 5 replies
  • 2 kudos

Resolved! Build error when integrating AI model to project

Hello, I am developing an AI classification model based on LSM6DSOX sensor data. Before adding the X-CUBE-AI software pack to Cube IDE, I was firstly developing the data acquisition code with the driver from X-CUBE-MEMS1, which I managed to do. After...

Resolved! Issues encountered when using STCubeAI

I want to run AI machine vision applications using STCubeAI. After training the model with TensorFlow components, I obtained a tflite file. Then, I imported and analyzed the model using the CubeAI toolkit in STM32CubeMX, and subsequently generated Cu...

Tokit_0-1711037026845.png Tokit_1-1711037082252.png
Tokit by Associate II
  • 1379 Views
  • 2 replies
  • 0 kudos