Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC5Studio expired license

Hi,I get this message when I open SPC5Studio: but I have already followed the istructions for Free Hightech license coping the new license in the requested folder.Does it means to have less functionalities with wizard to configure the MCU? 

clemyd78_0-1759506181936.png
clemyd78 by Associate
  • 668 Views
  • 1 replies
  • 0 kudos

Resolved! SPI Tx stucks on 1MHz clock

Hello All, I'm usin SR6P3 ARM mcu. I have to implement a simple SPI communication with StellarSDK. When send/receive starts the communication stucks in a while cycle where the code checks Tx queue busyness. while (queue->tx_busy == SPIQ_QUEUE_TX_BUS...

paduc77 by Associate
  • 1678 Views
  • 1 replies
  • 0 kudos

Resolved! SPC5 Studio sample, GHS build

I'm trying to build the SPC5 Studio SPC582Bxx sample project using GHS.I'm getting a lot of syntax errors in the *.s files.Do I need to manually fix these errors?What's the simplest way to build GHS?

image.png
John_Lee by Associate
  • 1528 Views
  • 1 replies
  • 0 kudos

SPC564A compatibility SPC563M

SPC564A datasheet promises compatability. Does that mean I can swap out SPC563M with SPC564A. Set target addresses in firmware, build and install, and all runs hunky dory?

Resolved! BSDL file for SPC58NE84

Hello,Where can I find the BSDL file for this device? The SPC58EG84 alternative should work as well.Thank you!

TubolyA by Associate
  • 967 Views
  • 1 replies
  • 0 kudos

Resolved! Stellar Studio for SR5E1E570C30F00X

Where can I find 'Getting Started' documentation for Stellar Studio - which is listed as SW dev tool for SR5E1E570C30F00X? For STM32 products, I was using STM32 Cube IDE which had Cube MX integrated (To generate driver code). I believe similar should...

sbagul by Associate
  • 634 Views
  • 1 replies
  • 1 kudos

Issues with FlashProgram at Large Block - SPC584Bxx

 Hello I'm trying to flash data on a large block, but I've seen that the current code stops with FlashErase or FlashProgram functions.So I tried flash control in two ways and none of them worked.1. divide separate section to flsh areas2. use the seco...

kitaehong_0-1757579382163.png

SPC5Studio Network ping application not working

SPC58EC-DISP: FreeRTOS+TCP “ping” demo never replies to ARP/ICMP (IRQ only fires periodically)Board: SPC58EC-DISP (DP83848 PHY)App note / demo: “SPC5Studio Network ping application” (AN5413) integrated into SPC5StudioHost: Windows PC, static IP 192.1...