User Activity

Hello community,I am using AEK-AUD-C1D9031 board and I want to play 2 audio files one after other. What should I change in the code?
Hello everyone,I have been flashing the code written in AutDevKit Studio 2.4.0 using UDE STK 2021 for the AEK-AUD-C1D9031, which uses the SPC582B60E1 MCU. I want to start debugging the code line by line using breakpoints.Currently, I have the option ...
While debugging the board AEK-AUD-C1D9031 , the SPC5-UDESTK is not responding and it says this always even when the target power supply is turned ON and the Device is shown in Device manager. I think there will be some target configuration which I ha...
Hello everyone, I am using the AEK-AUD-C1D9031 board along with AutoDevKit Studio 2.4.0 for programming. I imported the complete program file from the application library. When I tried to change the sound in the sounddb.s file, the board did not work...