Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Stellar SR6G7 HSM2HOST IE interrupt bit information

To enable the HSM notification to application core, I understood that we need to enable HSM2HOST IE register. I would like to know which bit position of 32 bit, we need to enable to make interrupt activate ? There is no such informations in the safet...

SPC563M-Disp

Hello,I have SPC563M-Disp development board, i am trying to flash hex file in it with the help of AEK-MCU-SSPC5LNKU tool. each time i try to connect my board with the SPC5-Flash-programmer it does not respond. Need support

SPC5 Flasher V2.8.1 not connecting to USB > Serial

Hello, recently downloaded SPC5 Flasher V2.8.1, this is required to flash a custom board using serial (RS232) to load the CAN-Bootloader (SPC564B74 @40Mhz), subsequent loading of programs is done via CAN. The SPC5 Flasher appears to be not connecting...

Quarryboss_0-1760699794171.png Quarryboss_1-1760700147194.png

Resolved! StellarStudio for Stellar SR6 P7 line

When I installed the the latest StellarStudio v8.0.0 (https://www.st.com/en/development-tools/stellarstudio.html#get-software), seems like it has installed the SDKs for Stellar E family only. How can I get the SDKs for Stellar P family. The link abov...

sg123 by Associate II
  • 377 Views
  • 1 replies
  • 0 kudos

SPC5-Flasher

Dear,I am trying to flash a SPC570S50E1 MCU through CAN. I have the SPC5FlashProgrammer software and a SH-C31A USB to CAN adapter. The MCU is flashed with "SPC570Sxx_RLA Bootloader Application for Discovery" example project from ST.The problem is tha...

SPC5 Chorus with 64GB EMMC memory

Hi, for a new project is search an MCU with 4 CAN FD and the possibility to connect a 64GB EMMC memory to safe data on it.Due to the harsh environment, a solution with an SD card is not possible. Do you know if i can connect it to the Bolero?Do you k...