Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Is it possible to not have a filter when receiving CAN messages?

Is it possible to not have a filter when receiving CAN messages? I want to create a gateway and transfer ALL messages from one CAN bus to another CAN bus. Do I just have to add 1000 messages to my list of allowed messages to ensure everything is acce...

PSing.5 by Associate II
  • 3022 Views
  • 2 replies
  • 0 kudos

SPC560B Flex CAN Flites

I am configuring the receiving filter of Flex CANHow to make it recognize only part of the IDFor example, the receiving ID is 0x123456You only need to identify 345 to consider the match successful

Jason Ren by Associate II
  • 2228 Views
  • 3 replies
  • 1 kudos

Resolved! FlashErase/FlashProgram not working with any optimization level (-Os size/-O1 general/-O2 speed/-O3 fast) except -O0 none.

Hi, I am working on SPC58NG84E7 bootloader. I have Bootloader code(at 0x00FC0000) with which i am using "FlashErase" API to Erase Flash Memory block at 0x00FF0000 with "-Os size" Optimization But its not working. Also, I tried putting breakpoint to t...

DMA by Associate II
  • 6525 Views
  • 14 replies
  • 0 kudos

BSDL for SPC56EL60L3?

Hello,I'm trying to perform Boundary Scan with a SPC56EL60L3 device but I can't find any BSDL file for these ICs in the ST website. Is there any available?Best regards,Mig

MigPol by Associate
  • 1026 Views
  • 0 replies
  • 0 kudos

Resolved! Use SPC5STUDIO with SPC584B-DISP Discovery kit

Hi,I'm planning to buy SPC584B-DISP Discovery kit and use the SPC5-STUDIO.but now, SPC5-STUDIO is in the ACTIVE state on the homepage, but GET SOFTWARE is not possible.Please let me know if this software is out of support or where I can download it.T...

yjin.1 by Associate II
  • 1672 Views
  • 2 replies
  • 0 kudos

Resolved! SPC5 Studio "Error: Unexpected Exception" error

Dear Community,Recently I want to learn SPC5 Studio environment. When I try to create new SPC5 application, I get "Error: Unexpected Exception" error. However I can create and compile sample applications. Can you tell me what is the problem? P.S. : I...

COnat.1 by Associate
  • 1544 Views
  • 1 replies
  • 0 kudos

Resolved! SPC584xx MCU Wakeup based on ADC

Hello,I am using SPC584xx MCU for an automotive application. One requirement in the project is to wake up the ECU when the analog voltage value read by the ADC crosses a threshold.Is this requirement possible to be implemented using SPC584xx MCU? Is ...

SKara.7 by Associate II
  • 1791 Views
  • 1 replies
  • 0 kudos