2021-10-21 12:40 AM
Hi community!
my name is Vincenzo,
I am looking, if any, for an example application that would help me understand how to send UDP messages from the SPC58EC-DISP board over Ethernet.
For the moment I have found an interesting application that allows me to ping the SPC58EC-DISP from my PC, but I'm not being able to do anything else. I noticed that there are demos available inside this application such as Simple TCP Echo Server, but I have not been able to get it to work. There is some documentation about it? besides AN5413.
Moreover, I would like to know if it possible to create the Ethernet socket to send a UDP message without using the FreeRTOS Component RLA component?
Thanks in advance for your support!
Vincenzo
Solved! Go to Solution.
2021-11-22 8:27 AM
Hello ,
There is no example for SPC58EC-DISP using Network component without FreeRTOS Component.
These components are dependent on FreeRTOS.
You need to recreate from scratch the Ethernet socket.
Best regards
Erwan
2021-11-22 8:27 AM
Hello ,
There is no example for SPC58EC-DISP using Network component without FreeRTOS Component.
These components are dependent on FreeRTOS.
You need to recreate from scratch the Ethernet socket.
Best regards
Erwan