Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Transmit SPI data from timer interrupt, the mcu become freeze

I tried to periodically send SPI data using PIT timer on SPC572.but whenever the timer interrupt call the SPI to transmit the data, the MCU freezing. while, when call the SPI transmit from main function, it working fine.any suggestion to solve this i...

jmary by Associate III
  • 3877 Views
  • 5 replies
  • 1 kudos

SPI IRQ delay

Hi all,I'm working on SPI communication between SPC582B and peripherals. I succesfully made it but I've found,  delay between characters sent by CPU is about 8us in 1MBit mode. Delay between last transmitted bit and tfff (transmit FIFO not full) is a...

Resolved! SPC5Studio FreeGcc ToolChain

Hi,i used SPC5Studio 5.8.1 for many years, but today (after windows update) in Properties->Tool Chain Editor->Current toolchain->"No ToolChain".This means that i have no possibility to change Build Settings. The same things also in SPC5Studio 6.Of co...

ck182 by Associate II
  • 5554 Views
  • 3 replies
  • 1 kudos

SPC584B Serial-Rx DMA Idle Interrupt

Hi. I am currently working on a project that involves implementing a data reception feature using the SPC584B-DISP board and the example application "RLA Serial DMA Test Application for Discovery 2."The objective is to efficiently receive approximate...

grantLim by Associate
  • 1511 Views
  • 1 replies
  • 0 kudos

Flash (NVM) of SPC564L70

Hi1) Is there specific document available for Flash (NVM) Access and Operation.2) What is the default value of NVM @ Power On?3) Error handling while programming the NVMThan you

SSJP by Associate
  • 1251 Views
  • 1 replies
  • 0 kudos

DMA-SPI-SPC58 DBE error

Hi guys,In my project, i am implementing DMA-SPI Tx/Rx for SPC58NH.Interrupt SPI is verified. Communication is checked.Problem is when i activate DMA for specific SPI channel, it triggers DBE(destination Bus Error).For example, DMA ch 12(DMACHMUX_0) ...

YJ_Joe by Associate
  • 1516 Views
  • 1 replies
  • 0 kudos

SPI Communication SPC58EC MCU

Hello,Currently I am working with SPI communication in SPC58EC DISP Discovery board. I wanted to evaluate communication between  MS-SL and SL-MS. I have configured SPID1 as master and SPID2 as slave. I was able to send data from master to slave using...

RSeba.2 by Associate III
  • 5644 Views
  • 6 replies
  • 0 kudos

Resolved! Does SPC560P44L3CEFAR have Flexray?

I am trying to configure flexray registers. But Controller is resetting when I access 0xFFFE0000, the address of MVR register. It is readable when I connect SPC5UDESTK in peripheral register window. I am using SPC560P44L3CEFAR mcu. Does it have flexr...