cancel
Showing results for 
Search instead for 
Did you mean: 

Can anyone help to tell me what is the meaning of the Marking H/G beside e3/e4 on the top marking of D2PAK component? Thanks

CPerf.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

As mentioned, the H stands for an internal information from the production of the device that has no influence on the behaviour of the STB37N60DM2AG and is therefore irrelevant for the user.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Welcome, @CPerf.1​, to the community!

Since you have not uploaded a photo of the components in question, one can only assume that this is internal additional information that is included with some D2PAK.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Peter,

Attached photo of the component mentioned can you help me identify the marking H?

Thank you.

As mentioned, the H stands for an internal information from the production of the device that has no influence on the behaviour of the STB37N60DM2AG and is therefore irrelevant for the user.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.