Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Standard CAN Message with DLC > 8 using SPC5 LLD

Hello,I know this is a bit of an edge case but during some testing today I noticed that the low level CAN drivers that come packaged with SPC5 studio only use the DLC field to work out how many bytes are in a recieved CAN the message. This isn't stri...

OHarc.1 by Associate II
  • 1852 Views
  • 1 replies
  • 0 kudos

Resolved! spc5-udestk license reset

I'm trying to install a license and change my computer.Please tell me how to reset license.Indicates that it is being used by another PC.

HJ.Goo by Associate II
  • 1553 Views
  • 1 replies
  • 0 kudos

Resolved! SPC5-UDESTK Code PC Reset

Dear valued customer,Your registration has been received.However these activation key------------------ and serial number ------------------ have already been used on another node by another users in another company.Since SPC5UDESTK are single-user n...

HJ.Goo by Associate II
  • 1667 Views
  • 1 replies
  • 0 kudos

Resolved! Bootloader not working with new SPC5Studio

Hi,I have troubles with the new version of SPC5Studio.I have made a bootloader with SPC5Studio V. 5.8.1 which is working fine but when I have remade it with the new SPC5Studio software it doesn't jump to application code. This is what happens: The bo...

FCola.1 by Associate III
  • 1876 Views
  • 1 replies
  • 0 kudos

Resolved! SPC58 StandbyMode : How to enter standby mode?

I use spc58nh-disp develop board.I want to enter the standbymode. but can't enter.If i setup SPCSetRunMode(SPC5_RUNMODE_STANDBY0) in main loop, It's behave.But after i get the RTOS, core0, core1 and core2 working, If i work SPCSetRunMode(SPC5_RUNMODE...

hans536 by Associate III
  • 1885 Views
  • 1 replies
  • 0 kudos

Resolved! OpenOCD works For Spc57 family?

I read from the OpenOCD docs in spc5 studio, I can only found sample instructions OpenOCD for spc58 family. But can't find any info about spc57 family support. Did spc5 studio openocd also working for other spc5 mcu family? 

jmary by Associate III
  • 2128 Views
  • 1 replies
  • 0 kudos

Resolved! SPC58 : how to measure execution time?

I use SPC58nh-disp.I use "time.h" and clock() function.but occur errorlike" c:/spc5studio-6.0/eclipse/plugins/com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.20200908161514/toolchain/bin/../lib/gcc/powerpc-eabivle/4.9.4/../../../../powerpc-eabivle...

hans536 by Associate III
  • 1897 Views
  • 1 replies
  • 1 kudos

Resolved! ELF File, what to do with it?

I am a bit too new to this St universe, could someone please point ,me in the right direction?I would like to update the Firmware on my BMS L9963 board. I found a folder on the website for the GUI for download. It contains a ELF file and some .dllsHo...

Orbiter by Senior
  • 3023 Views
  • 3 replies
  • 1 kudos

Resolved! Transmit SPI data from timer interrupt, the mcu become freeze

I tried to periodically send SPI data using PIT timer on SPC572.but whenever the timer interrupt call the SPI to transmit the data, the MCU freezing. while, when call the SPI transmit from main function, it working fine.any suggestion to solve this i...

jmary by Associate III
  • 3872 Views
  • 5 replies
  • 1 kudos

SPI IRQ delay

Hi all,I'm working on SPI communication between SPC582B and peripherals. I succesfully made it but I've found,  delay between characters sent by CPU is about 8us in 1MBit mode. Delay between last transmitted bit and tfff (transmit FIFO not full) is a...