Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Setup Output Pin for SPC582B PWM Emios

I want to generate pwm signal with spc582B with out the signal directly to pin emios0 channel 11 (uc11 pin).Already use the pwm Icu sample project. With channel 11 out, so I use group 1. When running, the periode callback is working, but still no out...

jmary by Associate III
  • 719 Views
  • 0 replies
  • 0 kudos

SPC58EC BMS Project : PIT Timers

Hello,As part of a custom BMS project, I am trying to add a cyclic CAN Message Transmission functionality to the board. I have been able to implement CAN transmission functionality on the main_core0 function where a function is called after every 500...

Vipuls by Associate III
  • 729 Views
  • 0 replies
  • 0 kudos

Changing start address at 0x011C0000 flash area

I’m trying to implement FOTA on SPC58NH, and changing the application start address is causing some issues.The 0x011C0000 flash block is not included in the boot record search locations.So I need to make the core start from this address, but I failed...

JYKim by Associate
  • 702 Views
  • 0 replies
  • 0 kudos

Resolved! Multi-core debugging on SPC58

I have been using SPC5-UDESTK with a STM58 evaluation board. I now need to start working with multiple cores, but it appears that the starter kit license does not support this functionality. Will the SPC5-UDEDEBG license allow for multi-core debuggin...

nullptr by Associate II
  • 1224 Views
  • 1 replies
  • 0 kudos

Resolved! Is SPE module discontinued for SPC58NN84E7?

Currently there is no appropriate documentation regarding the SPE module in the GTM. Is it discontinued? If anyone has a any good example regarding the SPE implementation or any application note regarding SPE. It would be helpful. 

vallabhd by Associate II
  • 1379 Views
  • 3 replies
  • 1 kudos

SPI with Very Strong Drive on SPC572L64

We used to have that working but now can only used weak or medium drive on the SPI pins (SCK & SOUT).Pin mapper or manual editing of the board.c file only gives us weak (0) or medium drive(1){(int16_t)MSCR_IO_INDEX(PORT_D, SCK_4), PAL_LOW, (iomode_t)...

Larsa by Associate III
  • 1414 Views
  • 2 replies
  • 0 kudos

How to use saradc with SPC570S

HelloI intend to use SARADC with SPC570S-DISP chip and I'm not able to operate correctly.I configured the saradc driver to use the pin ANP8, which corresponds to the board's potentiometer. I set up an interrupt to read the value. While the counter in...

SasukE15_0-1741165133376.png SasukE15_1-1741165185000.png
SasukE15 by Associate
  • 1582 Views
  • 1 replies
  • 0 kudos

Resolved! Newbie Tutorials

Good day ST community! I am a newbie in microcontrollers and only used arduino boards so far. I am looking for tutorials and manuals for fabricating a SPC570S40E1 microcontroller board and program it using  SPC5-UDESTK. I opened this case to the ST o...

Resolved! Help me for reading and write SPC570s

Hi, MY name is Metropolis and search support for reading and write this mcu. Mcu is spc570s, i'm search information on web and not have find. Thanks for you support, i'm search Data sheet correct and tools for reading and write. King Regard