Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! programming algorithm for SPC58

Hi Can anyone help in supplying the programming algorithm or programming specification for the SPC58 series chips.I want to program these on an In-Circuit tester without adding a special programmer.

Resolved! How can I configure interrupt (SPC560B54L5) without using Init package available (using just Platform RLA component) ?

I am using Init package component (in which irq, osal, etc. components are present). When I use just timer interrupt, it gets successfully run. however, when I am trying to add UART peripheral inside the code, it gets stuck at _IVOR1. What can be the...

SPI configuration in 32bits!!

Hi, Iam working on SPC560B60L5 In SPI configuration it is given that maximum frame size is 16. But I want to transmit 32bit data in a single frame, how should I configure it?

SEsak by Associate
  • 818 Views
  • 0 replies
  • 1 kudos

Unable to Enter into Halt Mode

Hi,I am trying to implement MCU sleep and wakeup mechanism using the MCU with the part number SPC560C50L3. I have developed a piece of code with reference to few reference documents(Reference Manual RM0017, AN4231, AN3316).In the sample code which I...

Resolved! Help for automotive grade mcu selection

Hi everybody,We are currently working on a commercial project for automotive industry. Since we are used to use ST mcus, we want to continue ST's automotive grade mcu. The requirements are listed below;- AEC-Q100 compliant- ASILB or higher level qual...

FErma by Associate II
  • 1474 Views
  • 1 replies
  • 0 kudos