2019-09-16 11:51 PM
Hello,
I am not able to activate the module entry in Clock Component RLA.
Can you please guide me how to do the configuration for sending the uc in standby mode.
Solved! Go to Solution.
2019-09-17 5:28 AM
Hello ,
There are 2 Test Applications
SPC560Dxx_RLA WKPU API Test Application for Discovery (STOP mode)
SPC560Dxx OS-Less STANDBY SRAM Test Application for Discovery (STANDBY Mode)
You can follow them with the RM0037.
The mecanism is the same
Best regards
Erwan
2019-09-17 5:28 AM
Hello ,
There are 2 Test Applications
SPC560Dxx_RLA WKPU API Test Application for Discovery (STOP mode)
SPC560Dxx OS-Less STANDBY SRAM Test Application for Discovery (STANDBY Mode)
You can follow them with the RM0037.
The mecanism is the same
Best regards
Erwan
2019-09-18 8:43 PM
Hello,
Are you able to set Standby mode in SPC560b now?
Because I am also facing the issue in setting standby mode.
Whenever i try to change the mode to standby it is going to STOP mode.
Please let me know if you resolved this issue.
Regards,
Rajesh
2019-09-24 6:37 AM
Hello Erwan,
I have used following line of code but the current drawn by the mcu is still 90mamp, for standby mode it should be in micro amp.
Kindly help me out with the issue.
uint32_t n =69;
uint32_t pctl = SPC5_ME_PCTL_RUN(2)|| SPC5_ME_PCTL_LP(1);
ME.PCTL[n].R = pctl;
ME.IS.R = 5;
uint8_t flag_ret = 0;
ME.STANDBY0.B.PDO = 0;
ME.STANDBY0.B.MVRON = 0;
ME.STANDBY0.B.DFLAON = 1;
ME.STANDBY0.B.CFLAON = 1;
// ME.STANDBY0.B.SSCLKON =
ME.STANDBY0.B.PLLON = 0;
ME.STANDBY0.B.OSCON = 0;
ME.STANDBY0.B.RCON = 0; //
ME.STANDBY0.B.SYSCLK = 0XF; //system clock disabled
// LOW POWER PERIPHERAL CONFIGURATION
//ME.LPPC[0].B.STANDBY0 = 0; //Peripheral is frozen with clock gated
//ME.MER.B.STANDBY0 = 1; //enabling the mode
ME.MCTL.R = SPC5_ME_MCTL_MODE(SPC5_ME_LP_PC_STANDBY ) | SPC5_ME_MCTL_KEY ;
ME.MCTL.R = SPC5_ME_MCTL_MODE(SPC5_ME_LP_PC_STANDBY ) | SPC5_ME_MCTL_KEY_INV;
while(ME.GS.B.MTRANS != 0)
Best Regards
Rewatee
2019-09-24 6:39 AM
Hi ,
I am not able to make exactly in standby mode.
Kindly help me out in case you resolved.
Regards
Rewatee