2019-09-11 2:12 AM
I am able to set STOP mode in SPC560B50l3 successfully, but still the total
current drawn is 6-7mA.
According to datasheet the maximum current consumed in stop mode under 55 °C is 500 uA.
Following is the code that i have added to set STOP mode:
ME.STOP0.B.PDO=1;/* Pad power sequence driver disabled, but state */
/* of the output is kept */
ME.STOP0.B.MVRON=0; /* Main Voltage regulator is off */
ME.STOP0.B.DFLAON=1; /* Data flash is in power-down mode */
ME.STOP0.B.CFLAON=1;/* Code flash is in power-down mode */
ME.STOP0.B.FXOSC0ON =0;/* Fast external crystal oscillator (4-16 MHz) off */
ME.STOP0.B.FMPLLON =0;/* FMPLL is off (default status during STOP0) */
ME.STOP0.B.SYSCLK=0xf; /* System clock disabled BEFORE RC switching off */
ME.STOP0.B.FIRCON =0;/* Fast internal RC oscillator (16 MHz) off */
ADC.MCR.B.PWDN = 1; /* Power donw analog part of ADC0 */
ME.MCTL.R = 0xA0005AF0; //request STOP mode
ME.MCTL.R = 0xA000A50F; //request STOP mode
while(ME.GS.B.S_MTRANS);
2019-09-17 5:41 AM
Hello ,
I forward your point to the good guy.
Maybe it is the way to measure.
Best regards
Erwan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.