Hi, Iam working on SPC560B60L5 In SPI configuration it is given that maximum frame size is 16. But I want to transmit 32bit data in a single frame, how should I configure it?
Hi, I'm using SPC560B54L5 Discovery board. I'm trying to get serial communication to work at baud rate 115200. And it works well with other baudrate like 9600,38400 and 57600.#define SPC5_PERIPHERAL1_CLK_DIV_VALUE 2U#define SPC5_LINFLEX0_CLK (S...