Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! How to check whether the SPC560B54L5 EVB IS IN STANDBY mode or not?

Hello,I am trying to make SPC560B54L5 EVB in low power mode that is STANDBY mode.The measured current in normal RUN0 mode is 143 mA whereas while keeping in STANDBY mode, it is around 92 mA. But as per the AN3316 Application note the max current cons...

0693W000000U6AvQAK.jpg
rpoon by Associate II
  • 1584 Views
  • 1 replies
  • 0 kudos

Resolved! How to use SPC560b54l5 discovery board to flash spc560b50l5 chip?

HI all, I am Ragu, and I need to flash SPC560b50l5 chip using SPC560b54l5 discovery board. I use PLS adapter setting in document as they mentioned but it not works?. Below I attached JTAG connection circuit diagram which I use. I probe the ...

Rpala.1 by Associate II
  • 2316 Views
  • 2 replies
  • 0 kudos

Resolved! How can I configure Simulink to compile for the SPC58-4B?

I have a SPC584B-DIS discovery board, and I can see that on the Matlab website it's listed as being supported hardware for Simulink.I have been trying to understand how exactly it should work though. I can see that most (all?)of the Simulink blocks a...

OGisl.1 by Associate
  • 2673 Views
  • 3 replies
  • 0 kudos

How to include Flash Driver into SPC5Studio project?

Hi,I am trying to include Flash Driver component into my project of SPC560B50L1.I have added it from available components and it appeared in project as shown on attached screenshot.Then I wrote simple procedure, but linker says that flash driver's fu...

0690X00000ButzFQAR.png
Yannek by Associate III
  • 4711 Views
  • 7 replies
  • 0 kudos

configure GPIOs at runtime; based on CAN message

HI, I am using SPC560b54l5 discovery board,I want to configure multiple GPIOs at runtime; based on the message received from CAN, when I configure particular pin as I/O by using pal_setgroupmode function but it not works, can anyone face this issue? ...

Rpala.1 by Associate II
  • 1353 Views
  • 1 replies
  • 0 kudos

Resolved! .bss section data corrupted

Hi All,We using SPC560P development board in our project. We saw board is halt program execution and checked .bss variable values corrupted. Could you please help me to understand this issue. Sharing my map file in attachment. EPWMD7 values are corru...

download.spc5studio.com

Dear All ,SPC5Studio updated components are available (56,57 on 58)more information on http://download.spc5studio.com/New or updated componentsRLA 1.12.0   SPC58ECxx : Machine check demo application   SPC58xHxx : OctalSPI driverNetwork 1.8.0New netwo...

Resolved! canbus transmission

I'm using the demo board SPC560P - DISP and the example SPC560Pxx_RLA CAN Test Application for Discovery .This Test Application use the CAN loopback, if I remove the flag of FlexCAN Enable Loopback in the can configuration setting I'm expecting to se...

gp73 by Associate III
  • 2420 Views
  • 2 replies
  • 0 kudos