2019-09-25 3:01 AM
Hi all,
I have downloaded the crypto lib directly from the "Help->Install New Software" menù of SPC5Studio , but I do not have any idea on how to use it, include it inside a project, use sample codes (if available), and so on.
Proposed link:
does not allow to download any library!!!
Could anyone be so kind as to help me? Any suggestions would be very appreciated!!!
Best regards,
Andrea Mocci
Embedded SE developer at Eldor s.p.a.
Solved! Go to Solution.
2019-09-25 3:08 AM
Hello ,
After installing SPC5-CRYPTO-LIB ,
There are a lot of samples code in the application wizard (Cf help Section)
Best regards
Erwan
2019-09-25 3:08 AM
Hello ,
After installing SPC5-CRYPTO-LIB ,
There are a lot of samples code in the application wizard (Cf help Section)
Best regards
Erwan
2019-09-25 3:11 AM
Hi Erwan,
Where can I find all these samples you're speaking about?
What do you mean with "CF help section"?
B.R.
Andrea
2019-09-25 3:24 AM
Ok Ok,
I've found same sample code (only for SPC560D platform).
Could this library be imported and used on different platform as SPC572L64E3 (Lavaredo) or SPC574K72E5 (K2)?
B.R.
Andrea