2023-02-20 08:25 AM
My test program for my STM32F746VET6 is extremely simple. Other than MX configuring the clock and GPIO, I only have a while loop that flashes some LEDS and then divides by zero.
while (1)
{
/* USER CODE END WHILE */
uint32_t bobbycounter = 0;
uint32_t bobbycounter2 = 0;
while(1) {
if(bobbycounter++ & 0x100000)
{
STATUS_LED_1_GPIO_Port->ODR &= ~STATUS_LED_1_Pin;
STATUS_LED_2_GPIO_Port->ODR |= STATUS_LED_2_Pin;
}
else
{
STATUS_LED_1_GPIO_Port->ODR |= STATUS_LED_1_Pin;
STATUS_LED_2_GPIO_Port->ODR &= ~STATUS_LED_2_Pin;
}
if(bobbycounter > 0x800000) {
bobbycounter = bobbycounter / bobbycounter2;
}
}
When I debug in MX, I get the expected behavior where I enter the HardFault_Handler and then flash the LEDS at a faster rate forever:
void HardFault_Handler(void)
{
/* USER CODE BEGIN HardFault_IRQn 0 */
/* USER CODE END HardFault_IRQn 0 */
uint32_t bobbycounter_hf = 0;
while (1)
{
/* USER CODE BEGIN W1_HardFault_IRQn 0 */
if(bobbycounter_hf++ & 0x10000)
{
STATUS_LED_1_GPIO_Port->ODR &= ~STATUS_LED_1_Pin;
STATUS_LED_2_GPIO_Port->ODR |= STATUS_LED_2_Pin;
}
else
{
STATUS_LED_1_GPIO_Port->ODR |= STATUS_LED_1_Pin;
STATUS_LED_2_GPIO_Port->ODR &= ~STATUS_LED_2_Pin;
}
/* USER CODE END W1_HardFault_IRQn 0 */
}
}
When I program a part using STM32CubeProgrammer, however, I never enter the HardFault_Handler. I don't have either watchdog enabled. What could be going wrong here?
Solved! Go to Solution.
2023-02-20 10:08 AM
> I'll try to look into other ways of forcing a hard fault if dividing by zero isn't a proper way to do it.
As Clive explained above, dividing by zero *is* a proper way to force a fault (which by default escalates to HardFault), but you have to enable it, by setting DIV_0_TRP in SCB_CCR, as it's by default cleared (and your debugger probably sets it - you may have a respective setting in your debugger for this).
Read PM0253.
JW
2023-02-20 08:34 AM
Typically that would be a UsageFault, if DIV_0_TRP is enabled. Would get the HardFault if escalated.
Perhaps the debugger is enabling things? Check CCR in non-failing case.
2023-02-20 09:50 AM
Thanks for the answer. Ultimately I just need a way to force a hard fault so I can test (my actual) function for reporting the cause. I have a much more complicated program that has evidence of going into hard faults sometimes. I'll try to look into other ways of forcing a hard fault if dividing by zero isn't a proper way to do it.
2023-02-20 10:08 AM
> I'll try to look into other ways of forcing a hard fault if dividing by zero isn't a proper way to do it.
As Clive explained above, dividing by zero *is* a proper way to force a fault (which by default escalates to HardFault), but you have to enable it, by setting DIV_0_TRP in SCB_CCR, as it's by default cleared (and your debugger probably sets it - you may have a respective setting in your debugger for this).
Read PM0253.
JW
2023-02-20 10:27 AM
Oh, gotcha. I misunderstood that part of his response.