cancel
Showing results for 
Search instead for 
Did you mean: 

NSRT_MODE and IRHEN option bytes are not configurable.

CTapp.1
Senior

I'm using V.2.16.0 to set the option bytes for the STM32G031, but NRST_MODE and IRHEN are not showing in the OB section.

There is a report for the same issue for the STM32G030 with the accepted solution being that the G030 does not officially support these options. However, that is not the case for the G031 as the options are documented in §3.7.8 of the reference manual.

1 ACCEPTED SOLUTION

Accepted Solutions
Amine_Jridi
ST Employee

Hi @CTapp.1 

Thank you for providing the Option Byte dump. Upon review, it has become clear that the differences in
the available options are attributed to the particular part number of the STM32G0 you are using which has 16K flash memory.
I have opened an internal ticket (Ticket ID: 181058) with our dev team to further investigate this matter.


I appreciate your patience and cooperation as we address this issue.

Amine.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
Amine_Jridi
ST Employee

Hi @CTapp.1 

I found the NRST_MODE and IRHEN options in the OB section for the STM32G031.

Could you send me an OB dump? you can use the following command with CLI: 

>STM32_Programmer_CLI -c port=<Portname> -ob displ

Thanks.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
CTapp.1
Senior

Sure:

------------------------------------------------------------------- STM32CubeProgrammer v2.16.0 ------------------------------------------------------------------- ST-LINK SN : 37FF680630484B3851221443 ST-LINK FW : V2J45S7 Board : -- Voltage : 3.57V SWD freq : 4000 KHz Connect mode: Normal Reset mode : Software reset Device ID : 0x466 Revision ID : Rev Y Device name : STM32G03x/STM32G04x Flash size : 16 KBytes Start Address : 8000000 Device type : MCU Device CPU : Cortex-M0+ BL Version : 0x54 UPLOADING OPTION BYTES DATA ... Bank : 0x00 Address : 0x40022020 Size : 108 Bytes [==================================================] 100% Bank : 0x01 Address : 0x40022080 Size : 4 Bytes [==================================================] 100% OPTION BYTES BANK: 0 Read Out Protection: RDP : 0xAA (Level 0, no protection) User Configuration: nRST_STOP : 0x1 (No reset generated when entering Stop mode) nRST_STDBY : 0x1 (No reset generated when entering Standby mode) IWDG_SW : 0x1 (Software independent watchdog) IWDG_STOP : 0x1 (IWDG counter active in stop mode) IWDG_STDBY : 0x1 (IWDG counter active in standby mode) WWDG_SW : 0x1 (Software window watchdog) RAM_PARITY_CHECK: 0x1 (SRAM parity check disable) nBOOT_SEL : 0x1 (BOOT0 signal is defined by nBOOT0 option bit) nBOOT1 : 0x1 (Boot from Flash if BOOT0 = 1, otherwise system memory) nBOOT0 : 0x1 (nBOOT0=1) Write Protection: WRP1A_STRT : 0x1F (0x800F800) WRP1A_END : 0x0 (0x8000000) WRP1B_STRT : 0x1F (0x800F800) WRP1B_END : 0x0 (0x8000000) WRP2A_STRT : 0x0 (0x8000000) WRP2A_END : 0x0 (0x8000000) WRP2B_STRT : 0x0 (0x8000000) WRP2B_END : 0x0 (0x8000000)
View more

In case it make a difference, I'm running under MacOS.

Amine_Jridi
ST Employee

Hi @CTapp.1 

Thank you for providing the Option Byte dump. Upon review, it has become clear that the differences in
the available options are attributed to the particular part number of the STM32G0 you are using which has 16K flash memory.
I have opened an internal ticket (Ticket ID: 181058) with our dev team to further investigate this matter.


I appreciate your patience and cooperation as we address this issue.

Amine.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Amine_Jridi
ST Employee

Hello @CTapp.1,

 

The issue has been fixed in STM32CubeProgrammer v2.18.

You can download it from this Link.

 

Thanks,

Amine.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
CTapp.1
Senior

Confirmed that this is now working as expected.

Thanks for letting me know it was fixed.