cancel
Showing results for 
Search instead for 
Did you mean: 

Generate srec file with option bytes configuration in offline mode?

STE_Michael
Associate II

Hello,

how can I generate a srec file with option bytes configuration in offline mode?
No St-Link and no hardware is connected!

STVP is an old tool which can do this simple things.

But it does not support all the microcontroller types (stm32Gxx).

Thank you for updating the version 2.15 to 3.0 ;)

 

 

 

 

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Maryem
ST Employee

Hello @STE_Michael,

Without connecting a device, it is not possible to read or write option bytes using STM32CubeProgrammer, as offline mode is currently unsupported. This means that generating the srec file with option bytes is also not possible. An internal ticket has already been submitted to the development team regarding your request.

Internal ticket number: 146447 (This is an internal tracking number and is not accessible or usable by customers).
I'll keep you posted.


Maryem.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Maryem
ST Employee

Hello @STE_Michael,

Without connecting a device, it is not possible to read or write option bytes using STM32CubeProgrammer, as offline mode is currently unsupported. This means that generating the srec file with option bytes is also not possible. An internal ticket has already been submitted to the development team regarding your request.

Internal ticket number: 146447 (This is an internal tracking number and is not accessible or usable by customers).
I'll keep you posted.


Maryem.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.