cancel
Showing results for 
Search instead for 
Did you mean: 

Error: No STM32 Target found! If your product embeds Debug Authentication,

Tajwar.Chandel
Associate III

Hi,

We are facing a issue to connect the ST link with our hardware setup ,,,, in today morning this is working fine but in afternoon facing the error in connection with the STlink debugger found error " Error: No STM32 Target found! If your product embeds Debug Authentication, please perform a discovery using debug Authentication." 

Target voltage showing :- 0 or sometimes 0.22v (after refreshing) 

TajwarChandel_0-1687180319452.png

Please suggest. 

11 REPLIES 11
AScha.3
Chief II

Hi,

0V from target: check voltage with dmm at your target, maybe it is really low.

You have any other target board, to check the st-link is working ok ?

 

If you feel a post has answered your question, please click "Accept as Solution".
FBL
ST Employee

Hello @Tajwar.Chandel 

Try to switch to Power down Mode in ST Link Configuration.

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Tajwar.Chandel
Associate III

Hi @Belaid,

Tried many times but still failed to connect. 

Hello Ascha,

We have facing the same issue on 2 numbers of boards from yesterday afternoon.

Regards,

 

hi,

not connected under power down mode as well.

 

Regards,

 

AScha.3
Chief II

>same issue on 2 numbers of boards from yesterday

so - you have many boards, and some working ok ?? or was it working before ?

If you feel a post has answered your question, please click "Accept as Solution".

Hi,

One more thing that this issue came after downgrade the firmware.

The MCU used STM32WB55RGV6.

Please suggest.

 

Regards,

Tajwar

Hi,

It was working before. 2 numbers boards down due to this issue. 

We have 1 more board that is working ok. 

Regards,

Tajwar

Sermed-65
Associate

same problem with two boards and no resolve problem?