2024-02-13 06:04 AM - edited 2024-02-13 06:05 AM
Hi everybody!
We have to implement firmware update feature via CAN interface. Our challenge involves implementing a secure and safe firmware update feature via the CAN bus, driven by regulatory requirements in the medical field. Unfortunately, the exact specifications are currently unknown.
I found X-CUBE-SBSFU and it seems like a great solution. However, I can't find any reference or example where X-CUBE-SBSFU is can be or used with CAN interface.
Is it possible to use the X-CUBE-SBSFU solution with CAN interface (by implementing "CAN loader" for example)?
Thank you in advance!
2024-02-19 01:46 AM
Did anybody have experience using X-CUBE-SBSFU with CAN bus?
2024-04-03 06:02 PM