Hi @bay
According to the messages in your console, drivers + middelware files among many others are missing.
I dumped my compilation console to compare it versus yours.
I suggest you to check which files are missing versus the ones in our TFM SBSFU ...
Hi @bay
There is no information in this snapshot that can help to understand the errors.
Can you start from the beginning of the console and copy the full messages ?
Best Regards
Hello @LVan .31 ,
There will be no issue in your case since the modification is performed before enabling the DMA (GPDMA_CxCR.EN=1 by calling HAL_DMAEx_List_Start ). We can't neither consider that the reconfiguration you did is dynamic for the same r...
Question 3/4:
Each STM32 Device has HW options bits that we need to program before using the device (known also as fuse in some communities).
In question 3 you are testing the HID example provided by the STM32CubeH7S package. It is working in debug m...
Hello @prometheans152
yes you can only generate the boot project: In the STM32CubeMx --> project manager --> keep the Boot project only.
The boot project will be loaded into the internal flash of 64 K. In general the internal flash is dedicated t...