cancel
Showing results for 
Search instead for 
Did you mean: 

The pin of FDCAN1, 2 does not exist on STM32h745/50 Discovery Board.

TLin.6
Associate II

Hello Community,

I would like to receive and transmit the data via FDCAN.

However, I cannot find the real pin on the STM32h745/50 Discovery Board.

The Microcontroller pin of FDCAN1_RX is PH14, PA11, PD0, PB8, and PI9.

The Microcontroller pin of FDCAN1_TX is PB9, PA12, PD1, and PH13.

0693W00000QKri0QAD.png0693W00000QKriyQAD.png0693W00000QKrmHQAT.png 

However, the pins cannot be found on the STM32h745/50 Discovery Board.0693W00000QKrntQAD.png0693W00000QKrpLQAT.jpgSo, how could I use the FDCAN1,2 pin and function...?

1 ACCEPTED SOLUTION

Accepted Solutions
Mike Lo
Associate II

Hi

I hope I can help with something. I believe, the microcontroller output pin configuration would be PH13 for TX and PH14 for RX for FDCAN1, but from this output it goes to the CAN driver U22, hence the output to HCAN and LCAN would have to be through CN11.0693W00000QKsQ2QAL.jpgBest regards

Mike

View solution in original post

2 REPLIES 2
Mike Lo
Associate II

Hi

I hope I can help with something. I believe, the microcontroller output pin configuration would be PH13 for TX and PH14 for RX for FDCAN1, but from this output it goes to the CAN driver U22, hence the output to HCAN and LCAN would have to be through CN11.0693W00000QKsQ2QAL.jpgBest regards

Mike

Hello Mike,

Thank you so much!