2024-03-29 11:06 AM
Hello!
I'm working with STM32G0B1 MCU and using CubeMX, I've enabled RCC_MCO for PA9 pin (HSI 16 source, 128 as prescaler) and a simple Input for PA8 pin. The code was generated to CubeIDE and "SystemClock_Config" function calls this method at the end:
HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_HSI, RCC_MCODIV_128);
But I noticed that both PA9 and PA8 outputs 0.125 MHz, even "MX_GPIO_Init" function setting correctly the pins!
Searching on HAL files, I found that "RCC_MCO1" defines to "RCC_MCO_PA8", so CubeMX should config MCO as "RCC_MCO_PA9".
Can we confirm this as a bug?
Solved! Go to Solution.
2024-07-08 01:55 AM
Hi @Pedro3 ,
Reported issue is fixed with STM32CubeMX 6.12.0, already available for use.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-02 06:41 AM
Hi @Pedro3,
Based on the description of HAL_RCC_MCOConfig, first parameter should have one of following values:
Could you please try replacing RCC_MCO1 by RCC_MCO_PA9?
I look forward for the result of this test on your side before making internal request for the fix.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-02 11:21 AM
2024-04-03 02:36 AM
Hi @Pedro3 ,
Thanks for your confirmation.
I reported this issue to development team.
Internal ticket number: 178119 (This is an internal tracking number and is not accessible or usable by customers).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-08 01:55 AM
Hi @Pedro3 ,
Reported issue is fixed with STM32CubeMX 6.12.0, already available for use.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.