2023-10-27 7:31 AM
When code for LINKEDLIST for STM32U575 will be generated (linked_list.c) with STM32CubeMX 6.9.2 several lines are missing. In the attached ioc file (which is only for illustrating the effect) the commands for e.g. setting DMA_DEST_DATAWIDTH_BYTE are missing before HAL_DMAEx_List_BuildNode(&pNodeConfig, &ByteCopy); on line 151 is called.
Solved! Go to Solution.
2023-10-27 8:09 AM
Hello @FB1
First let me thank you for your detailed explanation.
Issue is reported internally to our team (Internal ticket number:165108) and this will be fixed as soon as possible.
Thx
Souhaib
2023-10-27 8:09 AM
Hello @FB1
First let me thank you for your detailed explanation.
Issue is reported internally to our team (Internal ticket number:165108) and this will be fixed as soon as possible.
Thx
Souhaib
2023-12-19 10:11 AM
Is there an interim solution to this issue?
I'm encountering it as well and have posted a query here:
Thanks,
Andrei
2023-12-19 11:08 AM
Hi Andrei,
It works when in "LINKEDLIST Mode and Configuration" all entries are sorted according "Data Width", beginning with "Byte" then "Half Word" and so forth. There are small buttons "Move down" and "Move up" at the bottom.
Unfortunately it is not yet solved in MX 6.10.0 so this work-around, found by trial-and-error, is necessary.
Regards