2022-05-16 9:10 AM
With STM32CubeIde 1.9.0, open and change some settings in the IOC file, save your changes, and then click yes when a popup asks you to generate the code. At the end of the code generation, the IOC file is marked again as an unsaved file!
2022-05-19 8:50 AM
The file is modified by the build process!
Please go back through the earlier replies - it's been said before
2022-05-20 3:07 AM
Hello @MFred.2 ,
Thank you for having reported.
It seems that you're facing the same issue reported in this post, could you please check and confirm ?
Otherwise, could you please precise which MCU are you using and how did you exactly reproduced to observe this misbehavior ?
Thanks in advance.
Khouloud.
2022-05-20 5:17 AM
2022-05-20 5:37 AM
@Khouloud OTHMAN the other thread says there's an internal ticket on this.
Does that include addressing the problems mentioned above with revision control systems?
2022-05-24 7:03 AM
Hello @MFred.2 ,
Thank you for the clarification.
From my side I couldn't reproduce the issue with STM32U585.
In fact, hereafter the steps I've produced:
Following those steps, the project is always saved correctly and " * " will disappear from CRYP_AES_GCM.ioc tab.
Please correct me if I've missed something.
Otherwise could you please share you project for further check from my side ?
Your feedback is important to find the root cause of this misbehavior.
Khouloud.
2022-05-24 7:11 AM
@Andrew Neil , the internal ticket mentioned in this post is reporting the issue described in the thread but it will be updated accordingly if it is the same problem.
2022-05-30 5:49 AM