cancel
Showing results for 
Search instead for 
Did you mean: 

I need the consumed current value of Microcontroller part STM32F303ZET6. I am confused after checking datasheet. Please help.

KJ.4
Associate III
 
11 REPLIES 11

It's a complex multi-variable ​problem depending on what you're doing, the clock speeds, and a lot about what the pins are connected too and driving.

S​ome of the CubeMX tools can estimate what specific peripheral combinations contribute.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
AScha.3
Chief III

right, see in "Tools" in Cube...F303 -> at 48M + 72MHz

0693W00000aHQcKQAW.png

If you feel a post has answered your question, please click "Accept as Solution".
KJ.4
Associate III

I can see 40.71mA consumed at 72MHz.

Can I consider 40.71mA as the maximum current consumed by the IC?

those are estimates as @Community member​ said,

Depends of which peripherals youre using, i always design for 150mA minimum. for my stm32F072 and stm32F105

we dont need to firmware by ourselves, lets talk
KJ.4
Associate III

I am using 1 SPI, 2 UART & 1 I2C.

SCLK - 307KHz.

How much current to consider for STM32F303ZET6?

KJ.4
Associate III

If i consider IDD, then its 15.3mA( 8MHZ, Flash exe & All peripherals enabled)

If i consider IVDD, then its 160mA.

Which one to consider IVDD or IDD value?

@AScha.3​ @Javier Muñoz​ 

Please help here.

KJ.4
Associate III
 
KJ.4
Associate III
 

you just said your clock was 72Mhz, so the estimates are 77,4mA

we dont need to firmware by ourselves, lets talk