cancel
Showing results for 
Search instead for 
Did you mean: 

Examples not accessible in CubeMX for NUCLEO-L031K6?

MKosc.1
Associate

Hello,

I was trying to setup a prototyping project using the NUCLEO-L031K6 examples. But the current CubeMX version 6.7.0 does not seem so know about this dev board at all.

Is this a bug or is this nucleo board not fully supported by CubeMX?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Foued_KH
ST Employee

Hello @MKosc.1​ ,

Not All STM32 MCUs have examples with .ioc file in the Cube FW and STM32CubeMX don't provides examples for all MCUs.

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Peter BENSCH
ST Employee

Welcome, @MKosc.1​, to the community!

It is not a bug, the board is visible - at least on my machine. :grinning_face:

Have you installed the embedded software packages for the STM32L4?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Foued_KH
ST Employee

Hello @MKosc.1​ ,

Not All STM32 MCUs have examples with .ioc file in the Cube FW and STM32CubeMX don't provides examples for all MCUs.

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

MKosc.1
Associate

Hello,

thank you for the very fast replies! I seem to have misphrased the issue - the board is indeed visible as Peter pointed out and I can start a project based on it.

I just assumed the examples with associated .ioc files are commonly provided as well for all ST dev boards - thank you for pointing that out to me Foued.

I will proceed with the available configuration, just wanted to be sure I'm not missing something :)

yes sure you can share your project with me :D

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.