cancel
Showing results for 
Search instead for 
Did you mean: 

I have setup ADC1 & ADC2 for dual mode sampling in CubeMX for the Nucleo-H743ZI, when I change the input channel for ADC2 then Cube sets the "DMA Access Mode" to disabled for both channels. Is this normal behavior?

Wde G.1
Associate II
12 REPLIES 12
Wde G.1
Associate II

sorry didn't saw that one :grimacing_face:

Hi @Wde G.1​ 

Thanks for the feedback,

It is a normal behavior :

when we change the input (for example IN9 to ===> IN6), DMA ACCESS MODE still enabled.

0693W000000WqAqQAK.png

0693W000000WqC8QAK.png

When we unchecked IN9 for example then check IN6, DMA access mode change to Disable and to enable it you should go to ADC1 and change it to enable.

Best regards,

Nesrine

Wde G.1
Associate II

Thank you Nesrine!

If it's normal behavior then it ok once you know it ;)

Regards,

Walter.