cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743ZI I was trying to read multiple channels from ADC1 and ADC3. Using polling method i am able to get the values but when I try using DMA(HAL_ADC_Start_DMA(&hadc1,(uint32_t*) adc,6);) I am not getting any values.

MR.11
Associate II

In community they have asked to disable D cache (https://community.st.com/s/article/FAQ-DMA-is-not-working-on-STM32H7-devices). How to disable D cache globally. I made the necessary changes in the linker script. I am using system workbench for stm and stm32cubeMX.

DMA stream0 for adc1 6 channels.

DMA stream1 for adc3.

0690X00000D9468QAB.png

sample code

#include "main.h"

#include "usb_device.h"

/* Private includes ----------------------------------------------------------*/

/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/

/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/

/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/

/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

ADC_HandleTypeDef hadc1;

ADC_HandleTypeDef hadc3;

DMA_HandleTypeDef hdma_adc1;

DMA_HandleTypeDef hdma_adc3;

FDCAN_HandleTypeDef hfdcan1;

UART_HandleTypeDef huart3;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

static void MX_DMA_Init(void);

static void MX_ADC1_Init(void);

static void MX_ADC3_Init(void);

static void MX_FDCAN1_Init(void);

static void MX_USART3_UART_Init(void);

void MPU_RegionConfig(void);

/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/

/* USER CODE BEGIN 0 */

uint32_t adc[6],temp[6],adc2[6];

/* USER CODE END 0 */

/**

 * @brief The application entry point.

 * @retval int

 */

int main(void)

{

 /* USER CODE BEGIN 1 */

//char a[3]={'h','i'};

 /* USER CODE END 1 */

  

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */

 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */

 // MPU_RegionConfig();

 MX_GPIO_Init();

 MX_DMA_Init();

 MX_ADC1_Init();

 MX_ADC3_Init();

 MX_FDCAN1_Init();

 MX_USART3_UART_Init();

 MX_USB_DEVICE_Init();

 /* USER CODE BEGIN 2 */

 HAL_ADC_Start_DMA(&hadc1,(uint32_t*) adc,6);

 HAL_ADC_Start_DMA(&hadc3,(uint32_t*) adc2,6);

// HAL_ADCEx_Calibration_Start(&hadc1,ADC_CALIB_OFFSET, ADC_SINGLE_ENDED );

//   HAL_ADC_Start(&hadc1);

//

 /* USER CODE END 2 */

 /* Infinite loop */

 /* USER CODE BEGIN WHILE */

 while (1)

 {

  /* USER CODE END WHILE */

//   (HAL_ADC_PollForConversion(&hadc1,100));

//   adc[0] = HAL_ADC_GetValue(&hadc1);

//

//   (HAL_ADC_PollForConversion(&hadc1,100));

// adc[1] = HAL_ADC_GetValue(&hadc1);

  /* USER CODE BEGIN 3 */

 }

 /* USER CODE END 3 */

}

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen GH
ST Employee

0693W0000000EBCQA2.pngHello,

I have made a test to check and I don’t have any problem to read the values for ADC1 (DMA stream 0)

You should change the memory address, as shown in Figure (when using IAR)

Please see the RM0433 Rev 6 (page 101, 128) for more clarification

Best Regards,

MR.11
Associate II

Thank you.