2023-04-12 12:11 AM
2023-04-12 2:10 AM
Hello @vagar.1,
FMC is not suitable for interfacing directly with an ADC like the AD9235. You may need to check the datasheet for more details.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-14 1:00 AM
yes but i am trying with ads8598h
2023-04-14 1:20 AM
Hello again @vagar.1,
You may need to refer to the external ADC documentations to get more information. If the protocol requirements for the FMC parallel interface are supported for this peripheral, maybe it should work.
Have you tried to test it?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-14 1:32 AM
i am able to read the data but i am not sure that the data reading format is correct
2023-04-14 5:40 AM
@vagar.1, You may need to check the ADC configuration and check waveform, flags... for data reading format.
When your question is answered, please close this topic by choosing Select as Best the answer that answered your question or solved your problem. This will help other users find that answer faster.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.