DCT Issue: Missing HAL Interrupt Handler for USART6
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-08 5:20 AM
Hi everyone,
I'm encountering an issue with the STM32 Device Configuration Tool: it doesn't properly generate the global interrupt handler function for one of the UARTs in my project:
The generated interrupt handlers for USART1 and USART2 include call of the default HAL interrupt handler (HAL_UART_IRQHandler(&huartX);) but the handler for USART6 is missing this line.
/**
* @brief This function handles USART1 global interrupt.
*/
void USART1_IRQHandler(void)
{
/* USER CODE BEGIN USART1_IRQn 0 */
/* USER CODE END USART1_IRQn 0 */
HAL_UART_IRQHandler(&huart1);
/* USER CODE BEGIN USART1_IRQn 1 */
/* USER CODE END USART1_IRQn 1 */
}
/**
* @brief This function handles USART2 global interrupt.
*/
void USART2_IRQHandler(void)
{
/* USER CODE BEGIN USART2_IRQn 0 */
/* USER CODE END USART2_IRQn 0 */
HAL_UART_IRQHandler(&huart2);
/* USER CODE BEGIN USART2_IRQn 1 */
/* USER CODE END USART2_IRQn 1 */
}
/**
* @brief This function handles USART6 global interrupt.
*/
void USART6_IRQHandler(void)
{
/* USER CODE BEGIN USART6_IRQn 0 */
// missing from here:
/* USER CODE END USART6_IRQn 0 */
/* USER CODE BEGIN USART6_IRQn 1 */
/* USER CODE END USART6_IRQn 1 */
}
Project Details:
- Project: coprocessor_ica
- Processor: STM32F411CEU
- Configuration:
- 3 UARTs configured in the .ioc file (asynchronous mode, using DMA for both TX and RX)
- Global (and DMA) interrupts enabled for all three UARTs
- Using HAL drivers
Problem:
- The generated interrupt handlers for USART1 and USART2 include the default HAL interrupt handler call (HAL_UART_IRQHandler(&huartX);), but the handler for USART6 is missing this line.
Observations:
I have another project (coprocessor_vica) with the same processor and a very similar configuration.
- The main differences are the pin names and an additional timer configured in coprocessor_vica.
- In this project, the issue doesn't occur.
To investigate, I:
- Backed up the coprocessor_ica.ioc file.
- Copied the coprocessor_vica.ioc file into the coprocessor_ica directory and replaced all "vica" strings with "ica" using a text editor.
- After regeneration, the interrupt handler issue was resolved in coprocessor_ica.
- Renamed the pins and removed the extra timer to match the original coprocessor_ica setup.
- The issue reappeared.
- I created a new project from the original(ly faulty) coprocessor_ica.ioc in a different workspace, and generated the code. The handler call is still missing.
Questions:
- What could be causing this behavior?
- Are there any logs for the code generation process where I could trace where the issue occurs?
Environment:
- ST32CubeIDE:
- Version: 1.16.1
- Build: 22882_20240916_0822 (UTC)
- STM32CubeMX:
- Version: 6.12.1-RC4
- Build: 20240912-2256 (UTC)
- Platform:
- Apple M1
- macOS Sequoia 15.2 (24C101)
I've attached both .ioc files.
Thanks in advance for any insights or advice!
Solved! Go to Solution.
- Labels:
-
Bug-report
-
Interrupt
-
STM32CubeMX
-
STM32F4 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-08 9:59 AM - edited ‎2025-01-08 10:00 AM
@mÆŽALLEm
I found the cause, and it was (partly?) my mistake: in the System Core > NVIC > Code Generation tab, the Call HAL handler checkbox for the USART6 Global Interrupt was not checked. After enabling it, the code generation works correctly.
However, there are still a few things I don't understand:
- How could the checkbox become unchecked without deliberate user interaction?
- How is it possible that copying another working .ioc file and than modifying some pin names and enabling a timer also resulted in the same issue?
- How is it possible that the same .ioc file worked correctly for you? (I assume the checkbox is checked in your case if the generation works as expected.)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-08 5:36 AM - edited ‎2025-01-08 5:37 AM
Hello @tykhaytschaar ,
I'm not reproducing the behavior for both projects and HAL_UART_IRQHandler() is there:
Please use the latest version of CubeMx 6.13.0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-08 5:46 AM - edited ‎2025-01-08 5:53 AM
Thanks for the prompt response, @mÆŽALLEm .
In the meantime I tried to generate code on an ubuntu 22.04 machine with fresh installation of cubeIDE.
STM32CubeMX - STM32 Device Configuration Tool
Version: 6.13.0-RCS
Build: 20241122-0809 (UTC)
The issue occurs on this machine also.
Edit:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-08 5:54 AM
I don't have neither Ubuntu machine nor MacOS to reproduce the exact environnement as yours I'm on windows and didn't reproduce the behavior.
Did you download CubeMx from this link?
From where you downloaded the version 6.13.0-RCS ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-08 6:00 AM
I've downloaded official STM32CubeIDE installer from here: https://www.st.com/en/development-tools/stm32cubeide.html (chose "STM32CubeIDE Generic Linux Installer 1.17" exactly. CubeMX came as part of the IDE, so selecting RCS wasn't my decision.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-08 6:01 AM - edited ‎2025-01-08 6:14 AM
Ah! So try to generate the code from the standalone version of CubeMx 6.13.0 and see what happens. It could be an issue in the CubeMx version integrated in the CubeIDE.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-08 6:17 AM
I installed the standalone version of CubeMX on the ubuntu machine and tried generating the code with it as well. The issue still persists.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-08 6:19 AM
Could you copy your ioc file to another location and regenerate the code with the standalone version of CubeMx and see what happens?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-08 6:39 AM
I did, the result is the same.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-08 6:49 AM - edited ‎2025-01-08 6:49 AM
Ok since I don't have the same environment as yours I will escalate the issue internally so the teams will try to reproduce the behavior on the same environment. Internal ticket for follow-up: 199844 (not accessible by the community users)