cancel
Showing results for 
Search instead for 
Did you mean: 

DCT Issue: Missing HAL Interrupt Handler for USART6

tykhaytschaar
Associate II

Hi everyone,

I'm encountering an issue with the STM32 Device Configuration Tool: it doesn't properly generate the global interrupt handler function for one of the UARTs in my project: 

The generated interrupt handlers for USART1 and USART2 include call of the default HAL interrupt handler (HAL_UART_IRQHandler(&huartX);) but the handler for USART6 is missing this line.

 

/**
  * @brief This function handles USART1 global interrupt.
  */
void USART1_IRQHandler(void)
{
  /* USER CODE BEGIN USART1_IRQn 0 */

  /* USER CODE END USART1_IRQn 0 */
  HAL_UART_IRQHandler(&huart1);
  /* USER CODE BEGIN USART1_IRQn 1 */

  /* USER CODE END USART1_IRQn 1 */
}

/**
  * @brief This function handles USART2 global interrupt.
  */
void USART2_IRQHandler(void)
{
  /* USER CODE BEGIN USART2_IRQn 0 */

  /* USER CODE END USART2_IRQn 0 */
  HAL_UART_IRQHandler(&huart2);
  /* USER CODE BEGIN USART2_IRQn 1 */

  /* USER CODE END USART2_IRQn 1 */
}

/**
  * @brief This function handles USART6 global interrupt.
  */
void USART6_IRQHandler(void)
{
  /* USER CODE BEGIN USART6_IRQn 0 */
  // missing from here:
  /* USER CODE END USART6_IRQn 0 */
  /* USER CODE BEGIN USART6_IRQn 1 */

  /* USER CODE END USART6_IRQn 1 */
}

 

Project Details:

  • Project: coprocessor_ica
  • Processor: STM32F411CEU
  • Configuration:
    • 3 UARTs configured in the .ioc file (asynchronous mode, using DMA for both TX and RX)
    • Global (and DMA) interrupts enabled for all three UARTs
    • Using HAL drivers

Problem:

  • The generated interrupt handlers for USART1 and USART2 include the default HAL interrupt handler call (HAL_UART_IRQHandler(&huartX);), but the handler for USART6 is missing this line.

Observations:

I have another project (coprocessor_vica) with the same processor and a very similar configuration.

  • The main differences are the pin names and an additional timer configured in coprocessor_vica.
  • In this project, the issue doesn't occur.

To investigate, I:

  • Backed up the coprocessor_ica.ioc file.
  • Copied the coprocessor_vica.ioc file into the coprocessor_ica directory and replaced all "vica" strings with "ica" using a text editor.
    • After regeneration, the interrupt handler issue was resolved in coprocessor_ica.
  • Renamed the pins and removed the extra timer to match the original coprocessor_ica setup.
    • The issue reappeared.
  • I created a new project from the original(ly faulty) coprocessor_ica.ioc in a different workspace, and generated the code. The handler call is still missing.

Questions:

  1. What could be causing this behavior?
  2. Are there any logs for the code generation process where I could trace where the issue occurs?

Environment:

  • ST32CubeIDE:
    • Version: 1.16.1
    • Build: 22882_20240916_0822 (UTC)
  • STM32CubeMX:
    • Version: 6.12.1-RC4
    • Build: 20240912-2256 (UTC)
  • Platform:
    • Apple M1
    • macOS Sequoia 15.2 (24C101)

I've attached both .ioc files.
Thanks in advance for any insights or advice!

10 REPLIES 10
tykhaytschaar
Associate II

@mƎALLEm 
I found the cause, and it was (partly?) my mistake: in the System Core > NVIC > Code Generation tab, the Call HAL handler checkbox for the USART6 Global Interrupt was not checked. After enabling it, the code generation works correctly.

However, there are still a few things I don't understand:

  • How could the checkbox become unchecked without deliberate user interaction?
  • How is it possible that copying another working .ioc file and than modifying some pin names and enabling a timer also resulted in the same issue?
  • How is it possible that the same .ioc file worked correctly for you? (I assume the checkbox is checked in your case if the generation works as expected.)

tykhaytschaar_0-1736359144050.png