cancel
Showing results for 
Search instead for 
Did you mean: 

cubemx modify the project properties problem

Jisu Kim
Associate II
Posted on April 08, 2017 at 11:03

Hi. I'm using STM32CubeMX V4.20.1 and System Workbench for STM32(SW4STM32) now.

Actually I use CubeMX plugin for SW4STM32.

the problem is...when I click 'Generate Code' after changing the gpios or timers or any changes, project properties(more exactly Optimization) that I was set before changed after load the modified project.

I'll show you example pictures.

I think that is CubeMX V4.20.1's one of problem

#optimization #propertied #cubemx #sw4stm32
5 REPLIES 5
Imen.D
ST Employee
Posted on April 09, 2017 at 22:53

Hi Jisu Kim,

I will check this issue and report it internally if confirmed. 

We will keep you informed of any updates.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on April 10, 2017 at 00:47

Thank you!

Jeanne Joly
Senior III
Posted on April 12, 2017 at 17:06

hello

Kim.Jisu

,

I understand your point however, I can't reproduce it. When I change the optimization level in SW4STM32/Eclipse, the paremeter value is kept even if the project is reloaded.

On my point of view, the parameter optimization level is a parameter from Eclipse that is not given by CubeMX.

I wonder what arethe versions of your openSTM32IDE and ARM Compiler for MCU in Eclipse:

I have these versions :

0690X00000606apQAA.png

If you don't have the version 1.1.201701200843, please upgrade it and keep me informed if you still have the issue or not.

BR. Eric

Posted on April 12, 2017 at 17:36

Hello

Joly.Jeanne

‌!

Thank you for replying. My OpenSTM32IDE and ARM Compiler for MCU version is like below.

- OpenSTM32IDE : 1.0.201703061529

- ARM Compiler for MCU : 1.2.201703061592

I did reinstall CubeMX v4.1 but it didn't work too. So I installed CubeMX v4.0 and it fixed my problem.

well, I don't know what was problem, but now goes well. That's weird...

here's my eclipse installation details.

0690X00000606MnQAI.png

Thank you!

(and below link is my process? progress? when I did install CubeMX 4.1)

http://embejied.tistory.com/91

AlaaM
Associate III
Posted on July 10, 2017 at 14:29

I'm having the exact same issue.

CubeMX 4.21.0

OpenSTM32 IDE    1.13.1.201701200843

ARM Compiler for MCU    1.13.1.201701200843