Hello @Arman Ilmak ,
Dual-core debugging allows the simultaneous debugging of both cores.
(Both cores run individually or simultaneously from each of the GUI instances).
I advise you follow the steps for dual debug on MDK-ARM in the AN5286: STM32H7x5...
Hello @scaprile ,
Can you please share your ioc file?
You should check the valid path in your mx.scratch file and .ioc file input data?
ProjectManager.CustomerFirmwarePackage=
ProjectManager.DefaultFWLocation=
ProjectManager.FirmwarePackage=
Thanks
...
Hello @Mehul and Welcome to the Community
I advise you to connect under reset mode.
Check boot pin, NRST and SWD signal.
Also, make sure to upgrade the firmware.
Imen
Hello @EdgyAI,
Thank you for having reported the point.
Can you please share your ioc and log files for deep check.
I escalated this internally to CubeMx team in an internal ticket (ID 167860) to take a closer look at this issue.
(PS: ID 167860, is ...
Hello @PanosGial ,
Start the debugger separately for both cores: CM7 first and then CM4.
Set up the CM4 debug configuration following the order steps in this AN5361: Getting started with projects based on dual-core STM32H7 microcontrollers in STM32C...