cancel
Showing results for 
Search instead for 
Did you mean: 

BUG: Missing "Connect to running target" option in launch profile dialog

STMcubeIDE 1.1.0:

I'm using J-Link base to debug an STM32F413CG over SWD, which works well, but:

The launch configuration dialog is missing the "Connect to running target" option:

0690X00000Aqml9QAB.png

It should be included here like this:

0690X00000AqmlJQAR.png

When I create a launch profile using the Segger tool the launch fails with an error "Error while launching command: gdb --version" when I try to debug, though the GDB path, application folder, ELF, etc. all appear to be set OK.

@Markus GIRDLAND (ST Employee)​ - any idea how to work around these problems?

I do need to connect to a running target...

Please confirm the problem is understood and a ticket filed,

Thanks,

Best Regards, Dave

PS: If this isn't clear please see:

https://mcuoneclipse.com/2015/03/20/attaching-to-a-running-target-with-segger-j-link-gdb-and-eclipse/

1 REPLY 1

Anyone know how to connect to a running target using a Segger J-Link??

@Markus GIRDLAND​ ? Anybody else?

Thanks in advance for any pointers!

Best Regards, Dave