2019-10-23 8:22 AM
STMcubeIDE 1.1.0:
I'm using J-Link base to debug an STM32F413CG over SWD, which works well, but:
The launch configuration dialog is missing the "Connect to running target" option:
It should be included here like this:
When I create a launch profile using the Segger tool the launch fails with an error "Error while launching command: gdb --version" when I try to debug, though the GDB path, application folder, ELF, etc. all appear to be set OK.
@Markus GIRDLAND (ST Employee) - any idea how to work around these problems?
I do need to connect to a running target...
Please confirm the problem is understood and a ticket filed,
Thanks,
Best Regards, Dave
PS: If this isn't clear please see:
2019-10-24 3:35 PM
Anyone know how to connect to a running target using a Segger J-Link??
@Markus GIRDLAND ? Anybody else?
Thanks in advance for any pointers!
Best Regards, Dave