cancel
Showing results for 
Search instead for 
Did you mean: 

STLink Server with MacOS 15

jdw
Associate II

 

Hello,

I updated to Mac15 (MacOS Sonoma Public Beta), which was probably a mistake. Now I get an error from STMCubeIDE when I try to run indicating "ST-Link Server is required to launch the debug session" and to Please download it on www.st.com.  

I figured something changed in the OS that no longer makes the ST-Link Server run any more.

However when I try to download it, I get essentially a broken link, or at least it simply wont download. Even worse, the web page with Safari seems entirely broken and I cant even get a download to start after accepting the license, but with FireFox I get further, I get but still wont download and the link seems broke.

I can still flash using the STM32CubeProgrammer fortunately (using 2.13.1).

Can anyone tell me how to download this ST-Link Server? Or if there is an issue with the last MacOS and this and there is no fix?

 

33 REPLIES 33
tiny13a
Associate II

thanks so much. 

I can confirm that it DOES work with MacOS 15.1.1 and CubeIDE 1.17.0.

Updating from 1.16.x was a complete bust, there was an issue with the popup dealing with trusting various packages not having any content, then having to chase it across various monitors, then it wouldn't take clicks, so I just did a clean install of 1.17.0 and it just worked.

Thanks Rohdea, your sudo fix worked for me.

Does anyone know if there is now a 'proper' solution to this issue? 

I'm using Sequoia 15.1.1. I repeatedly got "ST-Link Server is required to launch the debug session" until I tried Rohdea's fix.

fsteiner
Associate II

Upgrading to STM32CubeIDE 1.17.0 (on MacOS Sequoia 15.1.1) solved the issue for me.