STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 441 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 323 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

How to program just a Single QSPI NOR Flash chip of STM32MP157c-EV1 using CubeProgrammer

STM32MP157c-EV1 is connected with two QSPI NOR flash chips.When programming NOR flash using the CubeProgrammer using tsv file, it automatically programs the two NOR flash in Dual-Flash QSPI mode.My requirement is to program just the Single Flash chip...

Resolved! Flashing STM32MP1 custom board over JTAG

Hello,I need to flash a custom STM32MP1 board which only has JTAG (no USB port available). Additionally, I build the image using Yocto meaning the output are separate binaries (e.g. U-Boot) and .tsv files.The STM32CubeProgrammer detects the CPU with ...

ANiko.3 by Associate II
  • 6774 Views
  • 12 replies
  • 0 kudos

Resolved! Cube IDE debug doesn't work on stm32mp157a-DK1

Hi,I'm having an issue while trying to debug the OpenAMP_TTY_ECHO_CM4 example described in gettin' started guide for stm32mp157a-DK1 (here link) using Cude IDE 1.4.2 on windows 10 machine. I configure the debug session as describe in the guide sectio...

MBassi by Associate III
  • 5369 Views
  • 11 replies
  • 1 kudos

Resolved! Cannot open 'console on MPU serial device'

I'm following the tutorials on the wiki about developing for the cortex-m4 on the DK2 kit. I'm facing trouble when I need to connect to the serial console, see image:The chars shown on the error message are random. Things already tried:Update ST-link...

0693W0000058zwgQAA.png
allard by Senior
  • 1507 Views
  • 1 replies
  • 0 kudos