STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 441 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 323 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

How to configure SDMMC Pin in STMCubeMx to make Board contain two SDMMC partitions both used for boot ?

Hello everyone, I'm configuring my STM32MP157C-DK2 Board pins and i want to make two SD Card partitions availabe. For the first one i chose the SDMMC1 and attributed it to PC10 pin for the second one do i need to choose SDMMC2 and to attribute it to ...

0693W00000AN55gQAD.png
FHami.1 by Associate
  • 2037 Views
  • 2 replies
  • 1 kudos

Resolved! Unable to boot from parallel NAND

Hello,I'm trying the NAND boot on our STM32MP157AAB3 custom board but until today I could't make the ROM code load the tf-a image from this memory.I'm yet able to boot from uSD (SDMMC1), eMMC (SDMMC2) and serial NOR (QUADSPI). For uSD I partitioned t...

RBors.1 by Associate II
  • 6369 Views
  • 3 replies
  • 0 kudos

Resolved! How to change the CPU clock frequency on STM32MP157F-EV1 board from 650MHz to 800MHz?

I noticed that even if I create a new project using STM32CubeMX IDE for STM32MP157F-EV1 board, in the clock configuration, the MPUSS_CK is 650MHz. In Linux, I can see the CPU frequency is 650MHz only. How can I clock the CPU to 800MHz as supported b...

New M4 project in cubeide has build button grayed out while running distribution package on STM32MP157c-DK2?

I am running the st-example-image-qt distribution package and am trying to use the M4 processor to feed sensor data to my UI. I can import the OpenAMP_TTY_echo example into stm32cubeide and debug it with my board fine. But now I am trying to make my ...

BSunw.1 by Associate III
  • 2156 Views
  • 2 replies
  • 0 kudos