STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is there a chance to perhaps get a video tutorials, of step-by-step for kernel-configuration-uploading ?

I have two codes running (on stm32mp157f-Dk2) successfully one is running on M4+freeRTOS another on A7+Linux, they are intercommunicating via RPMSGx. The problem is that after power-loss or reboot, I want both of my programs starting automatically an...

Resolved! C++ Compiler support on STM32MPU

Hi,I would like to compile a user space c++ application on the STM32MP157C-DK2. Is it possible to install GCC or G++ on the board?I tried installing them via apt-get but seems like there is not any package with name gcc or g++.How can i install it an...

NPal.2 by Senior
  • 1542 Views
  • 2 replies
  • 0 kudos

Resolved! The MDK uses OpenAMP to communicate.Loading is not initialized at /dev/ttyrpmsg0.Programs are available in the IDE.

 MDK compiles, and the program loads the following results: IDE compiles, and the program loads the following results: The MDK program is exported from the IDE, and the two programs are the sameI want to use openamp in MDK, how can I modify it

0693W00000Bd8ouQAB.png 0693W00000Bd8pxQAB.png
User.44 by Associate II
  • 926 Views
  • 1 replies
  • 0 kudos

LBEE5KL1DX-883 using SDMMC3

Hello,We are using the LBEE5KL1DX-883 WLAN+BT chip with a STM32MP157C on a custom board. The SDIO interface is routed to the SDMMC3 interface (different from the DK-2 board). However when we are probing the brcmfmac module, it cannot find the mmc0 in...

MLars.10 by Associate II
  • 2095 Views
  • 4 replies
  • 0 kudos

Resolved! Force re-compile local kernel changes

Hi,I have done certain changes to support the display in the dts files.I have modified dts files under kernel and u-boot.I had also added certain changes in panel-simple.c file as well. I gave a build and forgot to make some changes. So i changed tho...

NPal.2 by Senior
  • 2376 Views
  • 6 replies
  • 0 kudos

Resolved! Is there a way to load U-boot on STM32MP1 via dfu-util instead of STM32CubeProgrammer?

I want to use open source utilities to load U-boot into SRAM in "Serial mode". Is it possible?P.S. As I can see, there is an article about it on ST Wiki, but an access to it is restricted for regular users: https://wiki.st.com/stm32mpu/wiki/How_to_lo...

SNaza.1 by Associate
  • 1371 Views
  • 4 replies
  • 0 kudos