STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Custom compiled U-BOOT fail to boot from eMMC with ext4: ** Unrecognized filesystem type **

I have custom complied U-BOOT according this wiki page: https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package#U-boot_-_unpack_and_patch_sourcesIt was build succesfully to support QSPI flash. Now I want to unify i...

ASkri.1 by Senior
  • 7407 Views
  • 4 replies
  • 0 kudos

Resolved! DK1 EVB in production environment

Hello,Is there any clause from ST that prevent the usage of DK1 evaluation board in production? I have seen few notes in the user manual:https://www.st.com/resource/en/user_manual/dm00591354-discovery-kits-with-stm32mp157-mpus-stmicroelectronics.pdf"...

MToum.1 by Associate II
  • 3681 Views
  • 4 replies
  • 0 kudos

still unable to boot from qspi-nand

In addition to this question:https://community.st.com/s/question/0D53W00000pUh4gSAC/tfa-and-uboot-custom-compile-failsI'm still unable to boot from qspi. I addition to question about I've discovered, that it's necessary to add STM32MP_SPI_NAND=1 opti...

ASkri.1 by Senior
  • 9959 Views
  • 18 replies
  • 0 kudos

Change u-boot kernel command line

Hello there,I have a OSD32MP1-RED board based on stm32mp157c. Following the instructions How to create your own machine, I was able to compile the image. The problem happens when I try to boot from SD card with the generated image after load the boot...

MHern.4 by Associate II
  • 5328 Views
  • 2 replies
  • 0 kudos