STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP157d USART1

Hi,What am I doing wrong that USART1 returns -2 during the probekernel.dts -> PINS   usart1_pins_mx: usart1_mx-0 { pins1 { pinmux = <STM32_PINMUX('A', 9, AF7)>, /* USART1_TX */ <STM32_PINMUX('A', 12, AF7)>; /* USART1_RTS */ bias-disable...

Resolved! LPLV-Stop

Please tell me how to set the wake-up button (PA0:PWR_WKUP) as a return factor from LPLV-Stop mode and set STM32MP157f-EV1 to LPLV-Stop mode.

kiichi by Associate III
  • 4880 Views
  • 2 replies
  • 1 kudos

Resolved! stm32mp157dk2 Ethernet irq poll

Hi!I have been reviewing the kernel log for the DK2 Kit, and I have noticed that the Ethernet configuration is in polling mode. [ 37.074899] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [RTL8211F Gigabit Ethernet] (irq=POLL) Is ther...

AVazquez by Associate III
  • 1582 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP157 DK2 M4 debug issue

Dears,I'm using STM32MP157C-DK2 board in production mode.Now I'm debugging the firmware in M4 core. However, when I insert a breakpoint at DMA interrupt handler and wait for a while, it will crash the whole system (A7+M4) and lead to the reset.I also...

What does "RCC_HSE_BYPASS_DIG" mean?

Hi, I see STM32MP1 - M4 use "RCC_HSE_BYPASS_DIG", what does this mean? And from stm32mpcube, does anyone know the calculation below to get 209MHz?  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;RCC_OscInitStruct.PLL.PLLSource = RCC_PLL12SOURCE_HSE;RCC_...

Dat Tran by Senior II
  • 1067 Views
  • 1 replies
  • 0 kudos

Resolved! Graph is ploting slow in STM32MP1.

Processor Name: STM32MP157 Arm®-based dual Cortex®-A7 32 bits + Cortex®-M4 32 bits MPU Kernal Version: 5.10.10linux destro : openst linuxCrankstorybaord Version : 7.1OpenGLL Version : 2.0Screen Size : 1024 X 768I am developing medical GUI application...

NPal.2 by Senior
  • 1453 Views
  • 2 replies
  • 0 kudos