STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32mp135 boot stuck

NOTICE: CPU: STM32MP135F Rev.YNOTICE: Model: STMicroelectronics STM32MP135F-DK STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mp1-v23.06.21NOTICE: BL2: v2.8-stm32mp1-r1.0(release):custom()NOTICE: BL2: Built : 15:38:01, Jul 2 2025NOTICE: BL2: Bo...

Resolved! STM32MP257F-DK GStreamer problem

Hello,I'm using Buildroot environment with the STM32MP257F-DK board. I'm testing GStreamer with a simple pipeline:gst-launch-1.0 videotestsrc ! autovideosinkWhen I first run it there is no problem. The test video shows fine on the HDMI monitor. But w...

Ronte.1 by Associate III
  • 1980 Views
  • 6 replies
  • 0 kudos

Resolved! DFU mode stops abruptly

We have a custom design based on STMP32MP133A na an spi NAND. On paper, using the u-boot diagnostic commands, everything is working correctly.NOTICE: CPU: STM32MP133A Rev.Y NOTICE: Model: Zehnder CCPRO A1R Board INFO: PMIC version = 0x21 INFO: ...

angeloc by Associate
  • 1319 Views
  • 3 replies
  • 1 kudos

Resolved! no MPU with RGMII, FDCAN, 2x SAI ?

Heyho,I just checked the MCU selector in CubeMX (6.13), and to my surprise I didn't find any MPU supporting the following:gigabit ethernet (RGMII)FDCAN2 SAIs (I need at least 4 standard I2S/PCM "stereo" channels)The MP series don't have FDCAN.Then I ...

LCE by Principal II
  • 929 Views
  • 3 replies
  • 2 kudos