cancel
Showing results for 
Search instead for 
Did you mean: 

What is the function of PA13 (BOOTFAILN) on the STM32MP15x

RZ
Associate II

I'm working on a design with the STM32MP153 and came across the additional function of PA13 as BOOTFAILN.

I can guess what this means but I can't find any documentation on the subject. Don't know when or why this pin gets active. Or is it an input? In the reference design schematics both a LED and a switch are connected to this pin.

Thanks for any insight.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

please have a look to https://wiki.st.com/stm32mpu/wiki/STM32MP15_ROM_code_overview#Debug_and_Error_messages and also 8.3.5 "Debug triggers and LEDs" of AN5031

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here