User Activity

The output pin in question can be configured as LPTIM1_OUT and I know how to configure the LPTIM1 but I'm afraid I'll endup with LSE/2 as a clock. I need the LSE clock source to be connected to that output pin 1:1.Besides using the LPTIM1 isn't there...
Hi, I'm trying to make a headless system using the STM32MP153 and I would like to disable all graphical layers in the standard distribution.I'm using openstlinux-5.4-dunfell-mp1-20-06-24 (ECO V2 I believe)I have made my-own distro layer and was able ...
If I configure SAI 2 in cubeMX I get a greyed out option that the synchronous slave is not available unless I have one SAI as master, but I have set SAI A as master (or master with master clock out). So what am I doing wrong?It doesn't matter if I co...
I'm working on a design with the STM32MP153 and came across the additional function of PA13 as BOOTFAILN.I can guess what this means but I can't find any documentation on the subject. Don't know when or why this pin gets active. Or is it an input? In...
HW situation is:I2C2_SCL on PB10 (pin L4)I2C2_SDA on PB11 (pin M4)Both have a pull-up resistor of 18K.The sensor attached to these lines is removed, so nothing is connected.This is not a dev-board but our own design.I have generated code through STMc...
Kudos from