cancel
Showing results for 
Search instead for 
Did you mean: 

Display different application on HDMI and DSI at the same time

ALand.1
Associate

Hi,

I am building openstlinux-weston/st-image-weston image for stm32mp157c-dk2 board, and I have developed 2 application to be displayed at the same time. I configured DSI and HDMI with Buildroot, for the last one I followed this wiki: https://wiki.st.com/stm32mpu/wiki/How_to_display_on_HDMI, but I would like to know if there is a way to display 2 different application on the 2 interfaces at the same time.

Regards.

Aitor.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
PatrickF
ST Employee

Hi,

The STM32MP15x have a single display pipe (the LTDC) which could feed pixels to either pins (for parallel RGB LCD or HDMI converter) or internally to the DSI interface.

There is no way to have two images (same or different) on those two interfaces.

If you want a second display, you could have a look to use other serial interface (SPI, I2C) or parallel (FMC, exclusive to SLC NAND usage and not yet supported in SW deliveries). But for sure, resolution and refresh rate would need to be reduced.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
ALand.1
Associate

Thanks a lot.