STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Changing the eMMC pins with OTP

Hello,I have a custom board based on STM32MP151-C with an eMMC on the following pins:SDMMC2_CK PE3 (AF09)SDMMC2_D0  PE6 (AF07)SDMMC2_CMD   PG6 (AF10)I read that the ROM expects the the SDMMC2_D0 pin on PB14 so I need to change it by using values from...

ANiko.3 by Associate II
  • 7344 Views
  • 10 replies
  • 0 kudos

In ST-Link32 Utility, Read Out Protection is Disabled, but I get the errors: The elf loader Program function fails. Memory-Loader error Error occured during program operation Programming error @ 0x08000B60!

I have the latest version of ST-Link Utility (ver. 4.6.0) on Windows 10 and the latest firmware (V2.J37.S7), both of which I downloaded yesterday. My co-worker has ST-Link Utility ver. 3.7.0 on Windows 7 and firmware V2.J24.S7 and he has no trouble...

KLock.2 by Associate II
  • 1460 Views
  • 1 replies
  • 0 kudos

Hello I'm trying to write a loadable kernel module driver. I get an error during compilation: ERROR: modpost: "platform_device_alloc" [/home/rdm/ethtest/eth-ins.ko] undefined! Do I need something to set in the Kernel Config? Helloworld works as LKM.

#include <linux/platform_device.h>#include <linux/module.h#include <linux/types.h>MODULE_LICENSE("GPL");MODULE_AUTHOR("Robert W. Oliver II");MODULE_DESCRIPTION("A simple example Linux module.");MODULE_VERSION("0.01");static struct platform_device *pd...

NKorn.3 by Associate
  • 1416 Views
  • 1 replies
  • 0 kudos