STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is MDC mandatory for Ethernet?

I want to use a SIP with ST32MP153 and it uses PC13 to PMIC wakeup, PC1 is used for MDC so I'm left with only PI8 so can't use active tamper.I sit possible to use Ethernet without MDC so I can use PC1 for active tamper with PI8?

Oitsh.1 by Associate II
  • 2529 Views
  • 2 replies
  • 0 kudos

Is there a difference in operations when power on and when the SD card is inserted for the first time?

I use STM32MP151CAA3 Cortex-M4 on my custom board.I have created Linux image running on my custom board.​In the case that the SD card is inserted for the first time, Linux image is running successfully.However, in the case that I turn power off and p...

HMasu.1 by Senior
  • 2647 Views
  • 2 replies
  • 0 kudos